AXIS#.HOME.MODE
Description
AXIS#.HOME.MODE specifies the homing procedure of the drive. The homing modes available in the drive are summarized in the following table. See HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position for a detailed description of each mode:
Mode | Description |
---|---|
0 |
Current position |
1 |
Find limit switch |
2 |
Find limit switch then find zero angle |
3 |
Find limit switch then find index |
4 |
Find home switch |
5 |
Find home switch then find zero angle |
6 |
Find home switch then find index |
7 |
Find zero angle |
8 |
Find end stop |
9 |
Find end stop then find zero angle |
10 |
Find end stop then find index |
11 |
Find index signal, without any precondition |
12 |
Find home switch, including end stop detection |
13 | Absolute feedback |
14 | reserved |
15 | Find next feedback zero position |
16 | Find home switch using dual edges |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
Type |
Read/Write |
Units |
N/A |
Range |
0 to 15 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.HOME.MODE | 0x5008 | 0x2 | UINT | - | - | RW | False |
AXIS2.HOME.MODE | 0x5108 | 0x2 | UINT | - | - | RW | False |
Related Topics
Homing